Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Altivar 312 drive be powered up with an external control voltage?
Issue:
External control voltage to power up an ATV312 drive.

Product Line:
ATV312

Environment:
All serial numbers for ATV312

Cause:
To program the drive with external voltage

Resolution:
No.  The VFD needs full supply voltage to power and program the drive.