What SCADAPack E Modbus Client Method Should I use (Modbus Scanner or IEC Programming)?
SCADAPack E Modbus Client Operation
There are 2 methods to configure the SCADAPack E RTU to be used as a Modbus client. It can be done via IEC-61131-3 programs running on the controller, or it can be accomplished using the Modbus Scanner configuration in SCADAPack E Configurator. The method that you choose to implement depends on where the data you collect from the Modbus remote device is required
IEC 61131-3 Programs
Within IEC programs, there are an additional 2 methods. The legacy version uses the I/O devices to poll Modbus remote registers. A second method using Modbus set-up blocks was introduced in firmware 8.12.1. Both of these methods will return Modbus remote data into the IEC 61131-3 program variables. The data can be used in the programs for calculations and then applied to database points (using output I/O devices) if needed.
This method is useful if the Modbus remote data will be manipulated by an IEC 61131-3 program.
Modbus Scanner
A Modbus Scanner feature was also introduced in firmware 8.12.1. This lets a user configure Modbus polling within the SCADAPack E Configurator. Modbus remote data is returned directly into the SCADAPack E point database. If some of the data is needed in a IEC-61131-3 program, data can be mapped to program variables using input I/O devices.
This method is useful if the SCADAPack needs to act as a protocol converter between Modbus and DNP3 and/or the majority of the data will be sent to an upstream device as Modbus or DNP3.
Conclusion
Both methods can allow Modbus data to be used in IEC-61131-3 or converted to DNP3 points. The primary function of where the data will be used should be considered when choosing one of the 2 options.
Detailed operation of both methods is described in the SCADAPack E Documentation set (Included with the installation of SCADAPack E Utilities)
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.