Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SESU returns the error message 'Can't get to the Schneider Electric server' when trying to check on updates or and download updates for Unity..
Issue
This resolution provides an explanation on what could cause the Schneider Electric Software Update to fail when
trying to connect to the server to either check on updates or download updates for the Unity programming software..

Prouct Line
SESU

Environment
Windows 10

Resolution
If the Proxy Server settings is enabled in the Internet Explorer communications option page,  it will prevent the Schneider
Electric Software Update tool from accessing the server.  This will result in the error message 'Can't get to the Schneider
Electric server' to be returned.

To resolve the issue, disable the proxy setting.
frff