Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What may cause the New Variables from Equipment to be empty when linking the Vijeo Designer V6.2 variables to Unity Pro v?
When linking to a Unity Pro XVM or STU files, check that the IEC61131 box is checked in the Modbus Equipment driver configuration window.
Also check that there are no variable filters turned on. In addition, also check that the Unity project is built prior to export of the XVM file.