Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
You are using the PowerChute Agent to protect your Windows desktop machine with hibernation and/or sleep enabled and experience communication issues on wake up.

Issue:
You are using the PowerChute Agent to protect your Windows desktop machine with hibernation and/or sleep enabled and experience communication issues on wake-up.

Product Line:
PowerChute Business Edition 9.1, 9.1.1, 9.2, 9.2.1, 9.5, 10.x
PowerChute Serial Shutdown

Environment:
All supported Windows OS

Cause:
When connected to a Smart-UPS or Easy-UPS, hibernate and Sleep are not supported with PowerChute Business Edition or PowerChute Serial Shutdown.

Hibernate is supported when PowerChute Serial Shutdown is connected to a Back-UPS starting with version 1.2

Solution:
Disable Hibernate and or Sleep for shutdown in Power Options