Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum motor lead length you can run the ATV320 drive, without a load reactor?
Issue:
What is the max cable length you can run the ATV320 drive?

Product Line:
Altivar 320

Environment:
All

Cause:
Motor cable length distance without a load reactor.

Resolution:
The ATV320 drive can run up to 164 feet without a load reactor.
Cable length can go up to 164 ft without a reactor. If it's shielded cable we can go to 328 ft with a reactor. If it's  unshielded cable we can go up to 656 ft with the reactor.

Cable Characteristics (ATV320 Installation Manual page 75)

If you are using cables longer than 50 m (164 ft) between the drive and the motor, add output filters (for more details refer to the catalog). Use a shielded cable to meet the requirements of Category C2 or C3 according to the standard IEC 61800- 3, except when using a sinus filter. In this case, the use of a non-shielded motor cable is possible.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV320_Installation_manual_EN_NVE41289_05-pages-75.pdf [118.58 KB]