Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are some possible remedies for an Altivar 630 drive with an OSF supply mains overvoltage fault?

Article available in these languages: Spanish

Issue:
Clearing an OSF (Supply Mains Overvoltage) Fault on a Process Drive ATV630

Product Line:
Altivar 630

Environment:
All serial numbers for Altivar 630

Cause:
N/A

Resolution:
Some possible Remedies:
Check Line Voltage (L1, L2, L3)
Check DC Bus Voltage (PA+ to PC-)
Add Line Reactor
Continuous monitoring on Line Voltage to check for spikes or voltage dips (Scope Meter recommended)