Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why ATV-IMC with Drive ILF Error.
Potential issue:
An issue is present in the park due to a bad association between the Firmware and the Hardware.
Impacted ATV-IMC date codes are between 1537 - 1606.

The bad association is:
SoMachine V3.1
Old Firmware (Firmware =< to V1.1.2.13.) – New Hardware Date code > 1536
SoMachine V4.x
Old Firmware (Firmware =< to V4.0.1.13.) – New Hardware Date code > 1536


Behaviour of the card in case of bad Association
-    The Card works without issue ( But we cannot guarantee the behaviour in the time)
-    The card is in Error immediately after Run state.
Led Err are on.
No connection possible with SoMachine.

Cards impacted:
A list of serial number is joined in order to detect easily the cards impacted. See attachment for detailed list.
This list provides:
-    The Serial Number accessible on the Card.
-    The Serial number accessible on the Box

Action recommended
-   Ask for a replacement of the card by a new one, this exchange MUST done with the information:
-"Exchange for bad Firmware association"
-In the documents associated with the return.

Schneider Electric Egypt and North East Africa

Attachment(s)
Serial Numbers.xls [429.5 KB]
2016-06-01_1138.png [170.71 KB]