Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the power supply budget of the BMENOC03x1 modules?
Title
Power Supply budget  for the BMENOC03x1 module

Product Line
M580 BMENOC03x1

Environment
Unity Pro 11 or higher, Control Expert

Resolution
The Power Supply budget  for the BMENOC03x1 modules has been updated from 1.8W to 5.9W in Unity Pro V11.1 .
To update the Power Supply budget on Unity version 11 requires the installation of HotFix (HF0318000)