Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV930 drives have real time clocks?
Issue:
Is real time clocks built into the ATV930 drive?

Product Line:
ATV930

Environment:
All model numbers, all serial numbers

Cause:
Customer request

Resolution:
Yes, ATV930 does have a real time clock.  From the main menu, selects "My preferences" then highlights "Date/time settings" and presses OK.  This view allows to set date and time.  This information is used for the time stamping of all logged data.