Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to determine the actual current draw on the 'BMXCPS3540' power supply module using Unity?
Issue
Is it possible to determine the actual current draw on the 'BMXCPS3540' power supply module using Unity?

Product Line
BMXCPS3540

Environment
Windows 10


Resolution
No, It is not possible to determine the actual power supply current draw on the BMXCPS3540 M580 power supply module.