Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is Config ELEC?
Config ELEC is an application for Smartphone.
It is a tool used to configure the Wiserlink system with MIP or the Smartlink ELEC system
The configuration is a necessary step to ensure the proper functioning of your products/system.
In case of  WiserLink system, Config ELEC allows to:
- Make the pairing between MPR and MPE
- Set the pulse weight of the MPR and M2I
- Set alarms for M2I
In case of a Smartlink ELEC system, Config ELEC allows to:
- Configure and test the different inputs / outputs.