This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The LTMR offers two types of thermal overload protection - Inverse Thermal or Definite Time.
When you set the Thermal Overload Mode to Inverse Thermal and select corresponding motor trip class, then it has tripping curves according to IEC60947-4-1 - see Attachment1.
When you set the Thermal Overload Mode to Inverse Thermal and select corresponding motor trip class, then it has tripping curves according to IEC60947-4-1 - see Attachment1.
Released for: Schneider Electric Egypt and North East Africa


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.