Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the replacement temperature sensors for the ATS48 soft starters?
Issue:
Part number of temperature sensors for the ATS48 soft starters?

Product Line:
Altistart 48  ATS48

Environment:
All models

Cause:
Replacement

Resolution:
The replacement temperature sensor is selected based on the ATS48 part number.
There is one sensor per ATS48.
See the attached file.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATS48 Temp Sensor.pdf [187.97 KB]