Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to Convert a ProWORX NxT Project to ProWORX 32
This video will show you how to convert a ProWORX NxT project to ProWORX 32.

1 - Go to FILE > IMPORT > DATABASE
2 - Select the ProWORX NxT project to convert. It will have a .DCF file extension. Then click the OPEN button.
3 - ProWORX 32 will create a LOG file to show you if there are any conversion errors or warnings.
4 - Once the conversion is complete click the OK button.
5 - The ProWORX NxT project is now successfully converted over to ProWORX 32.