Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the XVU stacklight rated for outdoor application?
We don't recommend customers to use XVU for outdoor application.
The IP level (IP65) is not rated to UV protected.