Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would cause the ATV212 drive to ramp up to a partial speed, display retry and start up all over again?
Issue:
ATV212 ramping up to partial speed, then displaying retry and starting up all over again.

Product Line:
Altivar ATV212 and ATV21

Environment:
All

Cause:
Drive is resetting on phase loss or fault, and is trying to restart.

Resolution:
1st, check to see if the Auto Reset is enabled in parameter F303.  If it is ON, try turning it Off to see if the drive will give you a fault on the retry.
2nd, check to see if the input voltage on the Drive is balanced phase to phase and phase to ground.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center