Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does a preset speed override a standard frequency reference on Altivar drives?
Issue:
Wondering If a preset speed will override a standard frequency reference on Altivar drives

Product Line:
Altivar drives.

Environment:
All models, All serial numbers

Cause:
Clarification needed

Resolution:
Yes,  A preset speed will override a standard frequency reference when triggered.   When the preset speed is not being used, the drive will follow its standard frequency reference.