Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is SoMove 2.6.3 compatible with Windows XP?
Issue
Getting error message when trying to connect with SoMove

Product Line:
All Altivar Drives

Environment:
SoMove

Cause:
SoMove is no longer compatible with Windows XP

Resolution:
The last version that was compatible with Windows XP was SoMove version 2.1.24 - we do not support any newer SoMove version on Windows XP