Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
The Function Block ETH-PORT-CTRL is not able to control the enable/disable state of FTP and HTTP.
Issue
The Function Block ETH-PORT-CTRL is not able to control the enable/disable state of FTP and HTTP.

Product Line
BMXNOE0100

Environment
Unity

Resolution
Upgrade to the BMXNOE0100 firmware version 3.0 of greter