Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Generic_Modbus_DDXML_DTM_Library_2.0.3 documentation
Title
Generic Modbus DDXML DTM Library 2.0.3 documentation

Issue
Generic Modbus DDXML DTM Library 2.0.3 documentation

Product Line
Modbus

Environment
Unity

Cause
N/A

Resolution
The ReadMe file for Generic_Modbus_DDXML_DTM_Library_2.0.3 states that for devices supporting only Modbus serial line communication Process Data tab will not be available.
The Process Data tab is unavailable for device DTM which supports Modbus serial line protocol because some device DTM does not have Input/Output process data, as the DDXML does not contain the information for the process data. Attached is the documentation.

Schneider Electric Egypt and North East Africa

Attachment(s)
User Manual Generic_Modbus_DDXML_DTM.zip [3.44 MB]