[Unity Pro v11] Why the function block "ROL_DWORD" works incorrect in M580 platform?
Question:
Why the function block "ROL_DWORD" works incorrect in M580 platform?
It doesn't rotate the bit to the correct position. In other PLC platforms, it works well.
Answer:
This is a known issue on Unity 11 and it will be fixed on Unity 12.
Why the function block "ROL_DWORD" works incorrect in M580 platform?
It doesn't rotate the bit to the correct position. In other PLC platforms, it works well.
Answer:
This is a known issue on Unity 11 and it will be fixed on Unity 12.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.