Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the cause for A302 error seen on display of Lexium 32?

Issue:

What is the cause for A302 error seen on display of Lexium 32?

Product Line:

Lexium 32

Resolution:

A302 error is displayed when the digital input which is assigned as Limit Switch Positive (LIMP) has been interrupted.

The firmware monitors the limit switch inputs to prevent the motor from over-traveling when limit switches are used and assigned to the digital inputs.
If the limit switch for end of travel in the positive direction is faulty or has a intermittent connection to the drive then A302 will result.

Check all wiring related to the limit switch which is used to define the end of travel in the positive direction.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)