Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
LAN and WAN ports on the Easergy HU250

























In the Easergy HU250:

  • The "LAN" network interface is the physical double socket - number 5
  • The "WAN" network interface controls both the physical single sockets - number 3 (3rd party devices) and number 4 (SCADA)
With the V2.9 software, today, there is no separation of the IP traffic on these two physical ports.

It is technically feasible to do this, but it hasn't been implemented.

In the future:
As a gateway device, in order for  the T300 to keep the remote and local IP traffic separate, port 3 for third party devices will get its own interface e.g. LAN2

Schneider Electric Egypt and North East Africa

Attachment(s)
Easergy HU250 LAN AND WAN Network interfaces.pdf [45.24 KB]