Issue
Customer wants to use different protocol for each Ethernet port on the ION7400, PM8000 or PM5000 meter
Product
ION7400 series
PM8000 series
PM5000 series with dual Ethernet ports
Environment
Networking
Resolution
The ION7400, PM8000 and PM5000 meters with dual Ethernet ports have an internal Ethernet switch that is protocol Agnostic.
Each port can be used for different protocols such as ION and Modbus on ION7400 and PM8000, or Modbus and BACnet on PM5000.
Customer wants to use different protocol for each Ethernet port on the ION7400, PM8000 or PM5000 meter
Product
ION7400 series
PM8000 series
PM5000 series with dual Ethernet ports
Environment
Networking
Resolution
The ION7400, PM8000 and PM5000 meters with dual Ethernet ports have an internal Ethernet switch that is protocol Agnostic.
Each port can be used for different protocols such as ION and Modbus on ION7400 and PM8000, or Modbus and BACnet on PM5000.
Released for: Schneider Electric Egypt and North East Africa