Issue:
Communication options available on the Altivar 320 drives.
Product Line:
Altivar 320
Environment:
All serial numbers for Altivar 320
Cause:
N/A
Resolution:
Altivar Machine ATV320 drives with compact control block (ATV320-C) are equipped as standard with:
Altivar Machine ATV320 drives with book control block (ATV320-B) have been designed to simplify connections to communication buses and networks by means of the following:
Communication options available on the Altivar 320 drives.
Product Line:
Altivar 320
Environment:
All serial numbers for Altivar 320
Cause:
N/A
Resolution:
Altivar Machine ATV320 drives with compact control block (ATV320-C) are equipped as standard with:
- Integrated RJ-45 communication port for Modbus/CANopen
- The VW3A3600 mechanical adapter can be ordered separately for use with communication modules for additional protocols, see the list below.
Altivar Machine ATV320 drives with book control block (ATV320-B) have been designed to simplify connections to communication buses and networks by means of the following:
- Integrated RJ-45 communication port for Modbus/CANopen on the front
- Slot for an optional communication module
- Modbus TCP and EtherNet/IP (VW3A3616)
- PROFIBUS DP V1 (VW3A3607)
- DeviceNet (VW3A3609)
- EtherCAT (VW3A3601)
- POWERLINK (VW3A3619)
- ProfiNet (VW3A3627)
Released for: Schneider Electric Egypt and North East Africa