Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EGX100 and EGX300 China Compulsory Certification
Issue
Customer needs the China Compulsory Certification for the EGX100 and EGX300

Product Line
EGX100, EGX300

Environment
EGX 100 or EGX300 is being used for the gateway

Cause
Newer certification for an older device.

Resolution
An exemption was obtained for the China Compulsory Certification since these products are at their End of Life stage. See attached documents.

Schneider Electric Egypt and North East Africa

Attachment(s)
Signed_Contract_CCC_EGX.pdf [1 MB]
EGX100-300 for CCC exemption.pdf [127.3 KB]