Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are Power Monitoring Expert 8.0 licenses compatible with 8.1 and 8.2?
Issue
Upgrade from Power Monitoring Expert 8.0 to 8.1/8.2

Product Line
Power Monitoring Expert (PME) 8.x

Resolution
PME 8.0, PME 8.1 and PME 8.2 use the same licenses.