Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How configure VMWare in mode NAT and SoMachine for M251 communication via ETH 2 port
Use the following method with the VMWare configured in NAT mode:

1. Configure SoMachine the communication via "active path":

2.In the Communication Settings window , add a gateway and use the IP address of the
physique PC.

3.Select the new gateway and  Scan it

4. Now you can connect to the M251