Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference for 4 poles between 4P4D and 4P3D For NSX MCCB ?
For the 4 Pols MCCB of type NSX,

the main difference between 4P4D and 4P3D is in the neutral protection as follows:

- 4P4D: the neutral is Fully protected
- 4P3D: only the 3 main poles are protected while the neutral is not protected against any fault occurs inside it