Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is meant by the Flashing of the orange led in the front Panel of MCCB of type NSX ?
- For the MCCB NSX type,

the Orange LED in the front panel is the Pre-alarm default set for overload,

this LED is flashing when the flowing current is > 90 % of Ir as a pre-alarm for Overload soon condition