Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between UA and BA controllers used in Source change over system of NSX MCCB in the point of Load Shedding?
- For the Source change over system using MCCB of type NSX, in order to perform Load shedding and re-connection of on non priority loads,

This function is supported when using the Controller UA while it is not supported in the BA controller