Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Function of the interphase Barriers that are installed with NSX MCCB?

Safety accessories for maximum insulation at the power-connection points:

bb they clip easily onto the circuit breaker

bbsingle version for fixed devices and adapters on plug-in bases

bbnot compatible with terminal shields

bb the adapter for the plug-in base is required for mounting on plug-in and

withdrawable versions.