This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
- The TMD or TMG Thermal magnetic trip units that are used only with MCCB NSX of frame sizes 100-160-250 A are used only for Overload and short circuit protection and not ground fault protection.
- For ground fault protection, you can use:
1- Micrologic 6.2 (A/E) with NSX 100-160-250 A
2 -Micrologic 6.3 (A/E) with NSX 400-630 A
- For ground fault protection, you can use:
1- Micrologic 6.2 (A/E) with NSX 100-160-250 A
2 -Micrologic 6.3 (A/E) with NSX 400-630 A
Released for: Schneider Electric Egypt and North East Africa