How can we help you today?

Does the Sepam series 40 keeps the internal time in case of loss of the auxiliary supply?

Issue

A user wants to know whether a Sepam Series 40 relay retains its internal clock and stored data when the auxiliary power supply is lost.

Product

  • Sepam Series 40 Protection Relays

Environment

  • Sepam Series 40 devices operating with auxiliary power supply
  • Power outage or loss of auxiliary supply conditions

Cause

When the auxiliary supply is lost, the relay can no longer actively power its internal functions. Retention of the internal clock and disturbance recording information depends on the hardware design and backup energy storage components incorporated in the device.

Resolution

For Sepam Series 40 relays:

  • Units released before mid-2010:
    The internal clock is maintained by a capacitor for up to 24 hours following a power outage.
  • Units released after mid-2010:
    An additional capacitor was added to the design, allowing disturbance recordings to be retained for up to 48 hours after a power outage.

Additional information:

  • Sepam parameters and protection settings are stored in non-volatile memory and are therefore retained even when power is removed.
  • Other operational and event-related data are also stored in non-volatile memory. Refer to the applicable product documentation for details regarding the specific data types retained during a power outage.

Schneider Electric Egypt and North East Africa

Attachment(s)
Sepam 40 saved data.pdf [56.38 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center