Sepam SNMP implementation utilizes the industry standard MIB2 which provides information about the ACE850 communication module. ACE module only supports MIB2 because the information it provides is pretty basic which is why it does not require any MIB file. Please see the attachment for the list of information being provided.
Released for: Schneider Electric Egypt and North East Africa