How can we help you today?

What is the Sepam 80 IP raitng?

Issue

A user requires information regarding the Ingress Protection (IP) rating of a Sepam Series 80 protection relay.

Product

  • Sepam Series 80

Environment

  • Installation
  • Protection Relays
  • Electrical Panels and Switchgear
  • Equipment Enclosure Design

Cause

When designing or maintaining an electrical installation, users may need to verify the IP rating of the Sepam Series 80 relay to ensure the device is suitable for the intended environmental conditions and enclosure requirements.

Resolution

The IP rating information for Sepam Series 80 is provided in the product documentation.

Refer to the attached manufacturer documentation for detailed information regarding:

  • Front panel IP rating
  • Installation requirements
  • Environmental protection characteristics
  • Conditions applicable to the specified IP rating

The attached document contains the official IP protection rating specifications for the Sepam Series 80 relay.

Schneider Electric Egypt and North East Africa

Attachment(s)
TFR_201508150_001_sepam80_IP_test.pdf [863.95 KB]