Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a way in Sepam 40 to know the status of the breaker via communication?
A MES module is needed to read the status of the breaker and then the “circuit breaker control” function should be activated. Input I11 is used to monitor the open position while input I12 monitors the closed position. Then read the input via Modbus communication.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center