Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between the two ANSI protection functions 67N and 67P ?
For the Protection Functions:

67N: is used for earth fault directional overcurrent

67P: is used for 3 Phase Directional Overcurrent