Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
what is the rated Current For the Contactor LC1D09 if it works on AC1 Loads ?
The rated current for the contactor LC1D09 on 380 V AC if works with loads of type AC1 is 20 A