How can we help you today?

How do I test a Hot Standby PLC that is going to be a standalone system with I/O drop configured if the drop is not present?

Issue
How do I test a Hot Standby PLC that is going to be a standalone system with I/O drop configured if the drop is not present?

Product Line
EcoStruxure Control Expert, Modicon Quantum

Environment
140CPU67160, Control Expert v15.0


Resolution
A standalone Hot Standby PLC with a drop configured but not present will come up in Run Offline mode. In order to boot in Online set %S84 to 1.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center