Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What’s the definition of each bit of Setpoint Status Validity (Modbus Registers 2420-2421) in PM8240?

Issue
What is the definition of each bit of Setpoint Status Validity (Modbus Registers 2420-2421) in a PM8240?

Product Line
PM8000 Series

Environment
PM8000 Register List

Resolution
Register 2420

This register indicates which bits are currently active, or which bit-mapped inputs are marked as NA.

Bit 0 = Over I a - Validity (Status (Enabled or Disabled))
Bit 1 = Over I b - Validity (Status (Enabled or Disabled))
Bit 2 = Over I c - Validity (Status (Enabled or Disabled))
Bit 3 = Over I 4 - Validity (Status (Enabled or Disabled))
Bit 4 = Over V unbal - Validity (Status (Enabled or Disabled))
Bit 5 = Over kW sd - Validity (Status (Enabled or Disabled))
Bit 6 - Not Implemented
Bit 7 - Not implemented
Bit 8 - Not Implemented
Bit 9 - Not implemented
Bit 10 - Not Implemented
Bit 11 - Not implemented
Bit 12 - Not Implemented
Bit 13 - Not implemented
Bit 14 - Not Implemented
Bit 15 - Not implemented

Register 2421

This register indicates the current state of the selected input (either True or False).

Bit 0 = Over I a - Current State (True or False)
Bit 1 = Over I b - Current State (True or False)
Bit 2 = Over I c - Current State (True or False)
Bit 3 = Over I 4 - Current State (True or False)
Bit 4 = Over V unbal - Current State (True or False)
Bit 5 = Over kW sd - Current State (True or False)
Bit 6 - Not Implemented
Bit 7 - Not implemented
Bit 8 - Not Implemented
Bit 9 - Not implemented
Bit 10 - Not Implemented
Bit 11 - Not implemented
Bit 12 - Not Implemented
Bit 13 - Not implemented
Bit 14 - Not Implemented
Bit 15 - Not implemented


The following examples show the status and state of the Setpoint Modules for the related parameters using Data Mapping I/O Module.

Over I a
Over I b
Over I c
Over I 4
Over V unbal
Over kW sd

When all Setpoint Modules, including ‘Over I b,’ are disabled:

Setpoint Status and State-Disabled and Inactive

When only Setpoint Module 'Over Ib' is enabled with true state:

Setpoint Status and State-Enabled and true

In the first image, registers 2420 and 2421 display 0 for all bits, including Bit 1. Accordingly, the input registers, including Over I b, are marked as NA because the corresponding Setpoint Module was disabled.

In the second image, registers 2420 and 2421 display 1 only for Bit 1. This is because the setup register of the Setpoint Module 'Over I b' was changed to Enabled, and its output register indicates True, meaning the related alarm is active.