Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SoMachine vs SoMachine Basic

Article available in these languages: Spanish, French, Dutch

Issue:
Difference between SoMachine and SoMachine Basic

Product Line:
SoMachine, SoMachine Basic

Resolution:
SoMachine Basic is a free software created specifically to program the M221 Logic Controller exclusively.
It supports the Ladder and the Instruction List programming languages.

SoMachine is a full blown licensed software used to program a wide range of controllers like the M241, M251, M238, M258, LMC058, LMC078... as well as the Maglis HMIs.
It supports all of the IEC61131-3 programming languages.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: