Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will an ION8650 35S socket meter work in a 45S socket.

Issue:
User may have purchased a 35S socket meter and needs to connect it to a 45S socket

Product Line:
ION8650 Series Meter
Meter Socket

Environment:
Meter installation

Cause

How to wire an ION8650 meter 35 S socket in a 45S Socket as is not documented?



Resolution:
The 35S and 45S sockets are interchangeable. The ION8650 form 35S meter will function correctly in a 45S base.

35S Form 45S Form