Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the syntax / URL / script for opening directly an object from PLC application program accessible via webpage of BMENOC0311
The program viewer information should be enabled in the Unity application under tools > Projects Settings > PLC Diagnostics.
The firmware loaded in BMENOC0311 should be equal or above V2.07

The syntax / URL / Script is as follows
http://{IP_ADDRESS.EN_US}/#monitoring/plcpv?showConsole=0&showTreeview=0&section=Section_Name|Object_Name&standalone=1

Where IP_ADDRESS is the IP address of BMENOC0311.
SECTION_NAME is the name of the section used in the PLC program
OBJECT_NAME is the name of the variable used in the ladder logic program and is the object identifier in case of the FBD program

Schneider Electric Egypt and North East Africa