Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
At what temperature range can operate Schneider Electric servo motors?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

BSH and BMH motors can work in temperature range -20°C to 40°C (more with derating). SH motors operation temperature is +5°C to 40°C (more with derating). The reason are mechanical tolerancies in bearings and the grease that does not work at low temperatures.

Schneider Electric Egypt and North East Africa