Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION 8600 - Is it possible to disable Telnet?

Issue
Is it possible to disable Telnet on an ION 8600?

Product Line
ION 8600 Series

Environment
Meter Communications

Resolution
It is not possible to disable Telnet directly on the ION 8600. As a workaround, the port that the meter allows a telnet connection to, port 23, can be disabled on the network.

Updated note. The ION 8650 series has the ability to disable Telnet from within the meter settings.