Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use function block GMC.Control_ATV to control an ATV340 using a SoMachine PLC?
Issue:
Can I use function block GMC.Control_ATV to control an ATV340 using a SoMachine PLC?

Product Line:
SoMachine V4

Resolution:
You can use function block GMC.Control_ATV to control an ATV340 but you need to adjust the I/O mapping of the drive.
The I/O mapping of the drive can only be adjusted with the DTM commissioning software.
The library uses the assemblies 100 and 101 and requires the following mapping:
  • For assembly 100 (controller to drive):
    • First word: CMD (logic address 8501)
    • Second word: LFRD (logic address 8602)
  • For assembly 101 (drive to controller):
    • First word: ETA (logic address 3201)
    • Second word: FRRD (logic address 8604)
    • Third word: LCR (logic address 3204)