Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you protect the drive from users accessing menus on the ATV61 and ATV71 drive?
Issue:
Protect access of the ATV61/ATV71 menus.

Product Line:
Altivar 61, Altivar 71

Environment:
All

Cause:
Protection.

Resolution:
This function is available under 7.3.
You can either choose to protect or make invisible entire menus or select the parameters needed.