{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you run a single phase motor with an ATS22 or ATS48 softstart?

Article available in these languages: Spanish

Issue:
Wanting to run a single phase motor with an ATS22 or ATS48 softstart.

Product Line:
Altistart 22, Altistart 48

Environment:
All

Cause:
Single phase

Resolution:
No, there is not a single phase option for these product lines.  ATS48 and ATS22 are designed to run 3-phase motors only.

Schneider Electric Egypt and North East Africa